FB#.HALLMAP.U

Description

FB#.HALLMAP.U reads and writes to a mapping register used to correct mis-wired motors without physically changing the wiring. This keyword only effects feedback devices that have halls (see FB#.SELECT for feedback types with halls).

FB#. HALLMAP.U can be set to one of the following values:

Value

Description

0

The output is the U input value. (Default)

1

The output is the V input value. (Swap U with V)

2

The output is the W input value. (Swap U with W)

3

The output is fixed at 0.

4

The output is U input inverted value. (When input U=0, U output is 1)

5

The output is V input inverted value. (When input V=0, U output is 1)

6

The output is W input inverted value. (When input W=0, U output is 1)

7

The output is fixed at 1.

Versions

Action Version Notes
Implemented 02-10-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 7
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
FB1.HALLMAP.U

3500h

1bh

Unsigned8

-

-

Read/Write

No

FB2.HALLMAP.U

3501h

1bh

Unsigned8

-

-

Read/Write

No

FB3.HALLMAP.U

3502h

1bh

Unsigned8

-

-

Read/Write

No

FB4.HALLMAP.U

3503h

1bh

Unsigned8

-

-

Read/Write

No

FB5.HALLMAP.U

3504h

1bh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.HALLMAP.U

30740

7814

Unsigned8

Read/Write

-

FB2.HALLMAP.U

30741

7815

Unsigned8

Read/Write

-

FB3.HALLMAP.U

30742

7816

Unsigned8

Read/Write

-

FB4.HALLMAP.U

30743

7817

Unsigned8

Read/Write

-

FB5.HALLMAP.U

30744

7818

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.HALLMAP.U

30740

Unsigned8

Read/Write

-

FB2.HALLMAP.U

30741

Unsigned8

Read/Write

-

FB3.HALLMAP.U

30742

Unsigned8

Read/Write

-

FB4.HALLMAP.U

30743

Unsigned8

Read/Write

-

FB5.HALLMAP.U

30744

Unsigned8

Read/Write

-

Related Topics

FB#.HALLSTATE

FB#.HALLMAP.V

FB#.HALLMAP.W

FB#.SELECT